PSM Applications : FACTORY_TRIM_CRC_FAULT
Created by Michael Holloway on Sep 25, 2015
The device has an internal inconsistency in its EEPROM. This is often an indication the power was removed during a STORE operation or the device was incorrectly programmed.
Possible Causes:
- Power was removed during a STORE_USER_ALL operation before the write to EEPROM completed
- The device was programmed with data incorrectly
- One or more bits in the EEPROM have changed from their initial value
Remedies and Workarounds
- Avoid removing power during a STORE_USER_ALL operation until the operation is complete
- For an improperly programmed device, re-program the device 'in system' using the programming utility