The selected channel is Off. This may be due to a number of possible reasons.
Possible Causes:
TIP: Please use the 'Why am I Off?' tool in the upper right corner of LTpowerPlay for further insight. If you do not see the tool, click 'View > Restore Default Layout' in the menu. Below is a list of common reasons that a channel may be off:
- Commanded off via I2C
- Commanded off via logic pin (RUN/CONTROL)
- SHARE_CLK is not pulled up or pulled low, keeping the channel from turning on
- WDI_RESET is pulled low, keeping the IC in reset (this also prevents communication with the device)
- One or more faults configured as non-ignore may have occurred
- The GPIOB/FAULTB pin may be asserted low
- Vin may be below the programmable VIN_OFF threshold, which forces channels off