PSM Applications : UT_FAULT

A UT_FAULT was detected because the measured temperature was less than the UT_FAULT_LIMIT value. This fault applies to the die temperature on the 2977/2978 devices but is a paged fault on all other PSM devices. The OT/UT warning and fault limits and responses are global registers on the 2977/78 and are paged on all other PSM devices.

Possible Causes:

  • If the device is a LTC2977/78, low temperature was detected on either the internal die
  • Otherwise (all other PSM devices) this fault indicates low temperature was detected on an external temperature sensor on this PSM channel.
  • UT_FAULT_LIMIT set too high
  • A VSENSEP pin is floating
  • External TSENSE pin is floating

Remedies and Workarounds

  • If applicable, check for floating TSENSE pins and ground them
  • If a VSENSE pin is floating, it is possible that the internal die temp measurement is grossly in error, causing an OT or UT fault or warning. 

Other Debugging Tips

For 2977/78 devices, only an internal die temperature is available and therefore the OT/UT warn and fault limits are applied to the measured die temperature.  For all other PSM devices, the OT/UT warn and fault limits are paged and applied to each channel’s TSENSE pin; there are no internal die temp limits for these devices.